Can an external microphone be connected to the STEVAL-BCN002V1?
Using the pins on the underside that normally dock into the development board, to connect an external mic to the pins in order to get better recording?
Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Using the pins on the underside that normally dock into the development board, to connect an external mic to the pins in order to get better recording?
I need to make some modifications to the FP-SNS-ALLMEMS1 firmware for BlueCoin, but when compiling the project using STM32CubeIDE 1.9.0, the resulting firmware only works partially for getting streaming audio over BLE (BlueVoice in mobile app). I onl...
I have successfully designed a product which uses ISM330DHCX. However this unit only allows for a maximum of +/- 4000 dps, and within the application of the product, the gyro can saturate at high speeds.Are there any plans on releasing a product that...
Hi, I spend a lot of days trying to undestanding Microphones_streaming from X-CUBE-MEMSMIC1. That is very complex example and brillant at the same time. I want to extract the part for usb audio in streaming (device to pc), but it is a little crazy. i...
I have recorded hours of movement data using all three accelerometers (and gyro) of ST SensorTile.box sensor.In my custom application from expert mode, I set the ODR of LSM6DSOX on 208Hz, LIS3DHH on 1100Hz, and LIS2DW12 on 1600Hz. Output was set to s...
Hello,I am currently working with STM32wl55jc. My application invlolves few I2C sensors.The application also invlolves VL53l0x. These sensors have been mounted on a single PCB.I have tried explaining the problem below.1. I am currently reading the se...