MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Replace IMU sensor on an old PCBA with LSM6DSV320X

Hi We have a old PCBA design with a TDK IMU sensor. When I look at the footprint and pinout it seems like it actually drop-in-replaceable and we should need no new PCBA design, only change the BOM list and replace the TDK sensor with LSM6DSV320XBut t...

oysteikr by Associate II
  • 316 Views
  • 3 replies
  • 2 kudos

X-NUCLEO IKS4A1 with X-NUCLEO-6283A1

Hello,I'm facing some trouble with interfacing these two boards.Right now, I had only configured cube to load the datalogger example.It's running fine without the 6283A1 but when I plug it on the IKS4A1, the code crash.While debugging, I found that w...

AlexJ_0-1770305321464.png AlexJ_1-1770305463369.png
AlexJ by Associate II
  • 164 Views
  • 1 replies
  • 0 kudos

Multi FSMs on LSM6DSV16X

Hi, I am trying to merge the left and right wrist tilt configuration examples so that I have left wrist tilt on the FSM1 routing to INT1 and right tilt on the FSM2 routing to INT2 on LSM6DSV16X. I am sharing the merged config and the reference config...

a4ans by Associate II
  • 204 Views
  • 1 replies
  • 0 kudos

Resolved! SW_RESET on lsm6dsv16x bit is never cleared

Dear Community,I think I have encountered an uncommon problem. The SW_RESET bit in CTRL3 on the lsm6dsv16x does not change to 0 again. In https://www.st.com/resource/en/datasheet/lsm6dsv16x.pdf it states that after the software reset this bit is auto...

Resolved! STM32U575 and two PDM microphones on a single input

Hello,I have a PCB with two microphones (IM66D132HV01) with an STM32U575RGT6 (64pin) micro.Both microphones are connected (L+R) to a single input {PC0, PC2} = {MDF1_SDI4, MDF1_CCK1}Firstly I cannot find any example code that produces output samples i...

Looking for ST MEMS & motion sensors for project

Hello, I was told by the services to check out the forum for guidance.I am working on a project that requires surface reconstruction using non-optical based solutions. I was thinking of attaching a motion sensor module to track the handheld scanner w...