MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

memsmic1 on P-Nucleo-WB55

Hello, I am trying to use the MEMSMIC1 example on my nucleo-wb55 board, specifically the microphones streaming exampe to record sounds with audacity. I am able to compile and run the code. I am also able to see the microphone show up in the device ma...

Dead-reckoning over small distances with IMU sensor LSM6DSV16B

Hi,I'm trying to solve dead-reckoning over small distances and durations (few centimeters to few meters, over 2s to 20s approx. each time). After reading a lot of documentation ad publications, this seems pretty doable over small distances because th...

vchatelain_1-1713364439521.png vchatelain_0-1713364118048.png

LSM6DSV32X sensor hub mode magnetometer compatiblity

Evaluating the use of LSM6DSV32X + external magnetometer in sensor hub mode to achieve 9Dof. Is there a list of compatible magnetometers that should be used for this setup to work? Also is there  a pass through mode where we could talk directly to th...

IIS2DLPC interrupts not generated

HelloI have been trying to setup 6D orientation interrupt using IIS2DLPC and I am not getting any interrupts on INT1 pin when the orientation changes beyond threshold. For debugging I tried printing SIXD_SRC (3Ah)  and ALL_INT_SRC (3Bh)  registers. I...

KS.9 by Associate II
  • 3523 Views
  • 6 replies
  • 0 kudos

Resolved! NO DFU DETECTED - STWINKT1B

Hi guysI'm pretty new to the ST world. Just got my hands on an STWINKT1B, hoping to dive into its ultrasonic sound detection features. I spent today tinkering with it, trying to wrap my head around how it all works.So, I've got STM32CubeProgrammer in...

MTBF for LSM6DSO32TR

Hi, We are using IMU with part number LSM6DSO32TR in our application. Kindly provide us with LSM6DSO32TR details: 1) MTBF(Mean time between failures) 2) FIT(Failure in Time) 3) ROHS compliant (Certificate) I would be a great help!  

NIVI by Associate III
  • 1392 Views
  • 1 replies
  • 0 kudos

FP-SNS-DATALOG2 and macOS

I recently updated to a macOS and am have downloaded FP-SNS-DATALOG2 function pack and was going to use the HSDPython_SDK to log data from my STEVAL-STWINBX1, however it appears that macOS is not supported, is that correct?  No love for macOS or am I...

WP by Associate III
  • 2037 Views
  • 2 replies
  • 0 kudos

imu data synchronization

Hello, I'm working with the lsm6do. The lsm6dso is configured to 6,67kHz sampling rate of both, acceleration and gyro data. The INT1 pin will be set if gyro and/or acc data is available (INT1_CTRL = 0x03). In my application I'm polling the int1 pin (...

K-laus by Associate
  • 1167 Views
  • 0 replies
  • 0 kudos