Hi to All,I like to inform you that i am using the STM32F103RC controller and the problem is that when i do the DAC init between any of the peripheral init in STM32CubeIDE inside the main function, than i am getting the hard fault handler as shown be...
I have a text file full of values that I want to send to the DAC via the DMA. Is it possible to get the data through the DMA? I have tried opening the file using fopen and reading in the data to an array, and then passing the array to the DMA, but ha...
Greetings!I am new to microprocessors and am using an H7 board, and I have been using the CubeIDE. I have done most the basic/introductory examples, so I understand the basics of how to trigger the DAC with a timer, and how to run a timer in PWM mode...
Hi AllToday I wanted to start working with Bluepill DAC that turn out in STM32CubeIDE there is no DAC peripheral and I was shocked. Does anyone know what the h... is that issue? and how to solve it? I don't like to configure it by myself.
Hi, I am currently working on small project which I need to generate some arbitrary signal using DAC inside STM32G431KB.Code is shown below.#include "main.h" #include "SysClockConfig.h" uint16_t Output_Buffer[10] = {2048,2048,2048,2048,2048,2048,...
Hi,I am using Stm32CubeIDE v1.3.1 with my custom STM32F746IG board and touchGFX enabled (working properly with 800x480 paralel LCD). I have tried to play with DAC channels (Channel1-2). I can not get it work through the examples with DMA enabled or w...
Hello all,I need to use DAC on STM32F091 MCU. I have configured it in cubemx - Channel1 - output PIN PA4, output buffer enabled, no trigger.,in Main.c is next:static char dac_tmp=200;set_DAC_output(dac_tmp); if (HAL_DAC_Start (&hdac, DAC_CHANNEL_1 ) ...
Previously, CubeMX would reveal resource conflicts by hovering the mouse over the indicated area, e.g., GPIO pin configured as alternate function.Both version 1.0.2 and 1.1.0 do not indicate the nature of the conflict via mouse hover.To reproduce: C...