Error in initializing ST-LINK device. Reason: ST-LINK: Could not verify ST device! Abort connection.
Он выдает ошибку ошибки, которая указана в теме, как от нее избавиться, чтобы микроконтроллер можно было запрограммировать.
Он выдает ошибку ошибки, которая указана в теме, как от нее избавиться, чтобы микроконтроллер можно было запрограммировать.
Hello, I'm working on a project where I need to read the CAN bus messages that are coming from an ECU. I'm using the STM3210E-EVAL that has the STM32f103ZGT6. I'm reading the CAN bus messages with the following function: void HAL_CAN_RxFifo0MsgPendin...
I am using STM32f103 Controller ,In that i am trying to make complementary PWM output by using Timer 1TIM1 with PWM Generation CH1 CH1N ,But only gets the wave from this HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_1); function not getting other inverted si...
Dear team,We are currently in the process of designing a custom board centered around the STM32F103VET6 MCU. Unfortunately, we have been unable to locate a reference schematic that features this specific MCU. We kindly request the following informati...
HiI have the following problem on my STM32F103C8T for which I have no clue how to continue. I am running the ADC1 with DMA in continuous conversion mode scanning 6 input signals. Everything works fine. Next step was activating ADC2 triggered by TIM1 ...
Hi,"We are planning to design a custom board using the STM32F103VBT6TR microcontroller and are looking for guidance on how to set up the bootloader section in the schematics. Specifically, we want to enable the ability to reprogram the microcontrolle...
HiI am trying to get the blue pill detected on Ubuntu desktop , its now detected as LED Display board . Background I have flashed the blue pill on windows 64 but and trying to use the Bluepill on Ubuntu through wine , this board will act as the Softw...
Hello,I made a project using a blue pill. It works when is powered through st-link (3,3V).When I power this board from two AA batteries (~3V), the board does nothing until I press the reset button.An STM32F103 should work from 2 to 3,6 V, according t...
I am trying to read ADC from two channels without using DMA. For that I use this code: /* USER CODE BEGIN 0 */uint16_t ADC_VAL[2];void ADC_Select_CH1(void){ ADC_ChannelConfTypeDef sConfig = {0}; sConfig.Channel = ADC_CHANNEL_0; sConfig.Rank...
The below oscilloscope capture appears to show that disconnecting the ST-Link from the Windows laptop adds 80 ms to the NUCLEO startup, until the first UART packet is sent. If that is correct, what can cause this delay?Thank you in advance for your f...