cancel
Showing results for 
Search instead for 
Did you mean: 

Power on reset fails when I power a blue pill from batteries

xisco
Senior

Hello,

I made a project using a blue pill. It works when is powered through st-link (3,3V).

When I power this board from two AA batteries (~3V), the board does nothing until I press the reset button.

An STM32F103 should work from 2 to 3,6 V, according to its datasheet, or I need to adjust something?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

This thread relates to a so-called Blue Pill, which uses illegally cloned STM32F103. ST resources are only dedicated to supporting genuine ST products. We are not committed to ensuring that clones/fakes products work properly with the firmware we provide.

We recommend to purchase genuine products from STMicroelectronics and purchase them from known and trusted distributors.

This thread will now be locked. However, if you face difficulties while using genuine ST products, we’re here to assist you. Please feel free to start a new thread, and our team, along with community members, will be ready to help you with any issues/questions you encounter.

Thank you for your understanding.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
jiangfan
ST Employee

comments:

1. monitor the 3V (two AA batteries) with scope, to see if 3V voltage is stable during power on of the board

2. in case you have the source project, just debug it to see if it works as expected with power from the 3V (two AA batteries) supply

waclawek.jan
Super User

It's very unlikely that what you have on a bluepill is a genuine STM32, so the STM32 datasheet does not apply.

JW

Peter BENSCH
ST Employee

This thread relates to a so-called Blue Pill, which uses illegally cloned STM32F103. ST resources are only dedicated to supporting genuine ST products. We are not committed to ensuring that clones/fakes products work properly with the firmware we provide.

We recommend to purchase genuine products from STMicroelectronics and purchase them from known and trusted distributors.

This thread will now be locked. However, if you face difficulties while using genuine ST products, we’re here to assist you. Please feel free to start a new thread, and our team, along with community members, will be ready to help you with any issues/questions you encounter.

Thank you for your understanding.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.