cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F072B-EVAL SD card image

pawelr
Associate

Hi,

I am looking for a SD Card image from STM32F072B-EVAL kit. Without it demo program can not run. Package from ST site (en.stsw-stm32137) contains files from SD card, but it seems it does not work. I will be grateful for help.

1 REPLY 1
Peter BENSCH
ST Employee

Welcome @pawelr, to the community!

the STM32072B-EVAL is obsolete, but the firmware is still available. The STSW-STM32137 not only contains the media data for the SD card, but also the firmware for the STM32F072VBT6 in a file called stm32072B-eval_fw_v1.0.0.hex.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.