STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1431 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 560 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Update ARM toolchain in STM32Cube IDE

Hi,I wonder if it is possible to add/update manually the toolchain ARM?Currently it is only 7-2018-q2 while there is the 8-2018-q4 available.I wanted to use the latest one.Any ideas?Thanks in advance,Kind regards,Anthony

ABern by Associate II
  • 2232 Views
  • 2 replies
  • 0 kudos

SWV not working with STM32CubeIDE

Serial wire viewer is not showing since STM32CubeIDE version 1.0.1. It has worked before in version 1.0.0.I'm trying to use it with a STM32F103RBT6 but also tried it with a Nucleo F103RB.The live Expressions work perfectly fine, but not the SWV it ju...

0690X000009YQRbQAO.jpg 0690X000009YQRMQA4.jpg
thejc by Associate II
  • 3216 Views
  • 3 replies
  • 0 kudos

headless build fails when saving workspace

Hi all,I hope someone will be able to help me out. I want to compile my STM32CubeIDE project. It works but when it is saving the workspace, it returned an error. See below: Saving workspace.Stm32cubeidec:Java was started but returned exit code=1any i...

ABern by Associate II
  • 2355 Views
  • 4 replies
  • 0 kudos

"Make" path not found for stm32cubeIDE.

hello, while project build " make " path is missing.Error: Program "make" not found in PATHPATH=[C:/ST/STM32CubeIDE_1.0.1/STM32CubeIDE/jre/bin/server;C:/ST/STM32CubeIDE_1.0.1/STM32CubeIDE/jre/bin;C:/ST/STM32CubeIDE_1.0.1/STM32CubeIDE/jre/lib/amd64;]h...

barmy by Associate II
  • 1349 Views
  • 0 replies
  • 0 kudos

RTOS aware debugging in CubeIDE

I am contemplating a move over to CubeIDE from another commercial compiler and keen on the RTOS aware debugging (Using FreeRTOS) features.I have created a test project in CubeIDE but cannot see all these features (debugger views etc ) listed in the p...

JamesP by Associate
  • 1628 Views
  • 1 replies
  • 0 kudos

Unable to build a project clones from gitlab

I have cloned a project into ,y system and I opened the main.cpp file to build and check the code but I'm unable to find the build option. Also I nedd to debug using segger. Can someone please help me pout as I'm new to this and I'm very keen on lear...

PSoma by Associate
  • 705 Views
  • 0 replies
  • 0 kudos