STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1463 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 569 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

System States "Code generation could not be done because the necessary firmware package is missing. Not able to complete STM32Cube project creation."

I have loaded all of the tools, this includes STM32CubeMX and STM32Cube IDE. I purchased the STM32F303RE Eval board to start project flow. The system states it was denied access to my C:\ drive. Instructs me to look at "Firmware Update" concening pac...

TFlac by Associate III
  • 1151 Views
  • 1 replies
  • 0 kudos

Hi, I have an STM32F413ZH Discover board.I have imported FREE RTOS on to the board.Now I have been trying to implement LOW POWER mode in it.For that I have enabled the macro configUSE_TICKLESS_IDLE to 1. But even though the low.

I have tried calling the function HAL_PWR_EnterSLEEPMODE function call also but even though the Controller is not entering sleep mode.I want to know how to configure the sleep mode in the FREE RTOS for this controller.RegardsSrikanth.

Smedi by Associate II
  • 1224 Views
  • 2 replies
  • 0 kudos

How to debug code on external flash?

I'm trying to debug code in external flash memory mapped at 0x90000000. However, I get the following error when looking at the disassembly during debug. Failed to execute MI command: -data-disassemble -s 2415922564 -e 2415922663 -- 3 ...

STM32CubeIDE + STM32F7 + LwIP does not build

HelloI'm working with STM32CubeIDE ver1.0.2 and STM32F7508-DK.(F7 Hal Fw version : 1.15)I'm trying to Eth, LwIP.When I generate basic code with LwIP configuration, CubeIDE cannot build, has error.error message is [makefile:45: projectname.elf] error ...

J.Park by Associate II
  • 1028 Views
  • 0 replies
  • 0 kudos

Resolved! How to uninstall it?

I've tried to uninstal it from Windows7 standard "programs and components". It's said that the "Program has already been uninstalled, remove from the list". But nothing actually has changed. Now I can't reinstall the IDE cause the installer argues th...

Ruslan1 by Associate II
  • 5474 Views
  • 3 replies
  • 0 kudos