2019-07-30 10:22 PM
if i Migrated a sample project from Keil Uvision to STM32Cube IDE. What changes do i need to do in that project to fit for the STM32Cubde IDE
thanks
Solved! Go to Solution.
2019-08-02 5:20 AM
My official recommendation is to wait to migrate to CubeIDE until you have a new project and not migrate as it's not guaranteed to work.
However.... :smiling_face_with_halo: you should be able to use the methods used for migrating IAR projects to TrueSTUDIO and probably manage to get it to work with CubeIDE since they are pretty similar.
I haven't tried it myself and I'm not sure if it's possible, but if you want to try then here is the manual for how to do it in TrueSTUDIO.
2019-08-02 5:20 AM
My official recommendation is to wait to migrate to CubeIDE until you have a new project and not migrate as it's not guaranteed to work.
However.... :smiling_face_with_halo: you should be able to use the methods used for migrating IAR projects to TrueSTUDIO and probably manage to get it to work with CubeIDE since they are pretty similar.
I haven't tried it myself and I'm not sure if it's possible, but if you want to try then here is the manual for how to do it in TrueSTUDIO.
2019-08-02 6:00 AM
First of all thank you for this Guide!
Can i have a follow up question, do you have any guide there for migration from f4 to l4?
2019-08-03 3:02 AM
Thanks for this recommandation. Since the CubeIde relaase, I was wondering if I have to migrate my TrueStudio Project.
I spend and lost a lot time after while I roll back to TrueStudio. I had a lot of trouble with project configuration, virtual folder include issue. Unable to compile properly.
I will stay on the TrueStudio last release until a real major relaease of CubeIde.
Bertrand
2019-08-05 1:18 AM
Maybe such a guide exists somewhere but it's not a guide we made at previous-Atollic so I can't link you anything about it.