STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1451 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 568 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Looking for a comprehensive PDF for STM32CubeIDE. There is a nice video on STM32CubeIDE located on the ST website showing many neat things but?

I am new to STM32 world and all of its tools. I have purchased a STM32F303RE board and downloaded the STM32CubeMX and STM32CubeIDE. I also downloaded SW4STM32 as many ST User manuals contains many examples for this IDE tool. After two weeks of playin...

TFlac by Associate III
  • 1427 Views
  • 2 replies
  • 0 kudos

Resolved! Can't select FreeRTOS for my STM32F103 board

When I installed at first CubeIDE, I could select FreeRTOS as middleware. But failed due to can't use systick as reference clock of FreeRTOS.After that, I can't choose a Middleware such as FreeRTOS, when I create New Project.What am I wrong?

Clee.4 by Associate II
  • 1099 Views
  • 1 replies
  • 0 kudos

Nucleo-H743zi standard output to the STM32CubeIDE console

I have a Nucleo-H743zi board and am debugging an application using STM32CubeIDE. There is some legacy code that does some debug printf's I don't see anything on the debug console or the regular console. How does one configure standard output to r...

MRait.7 by Associate
  • 2048 Views
  • 4 replies
  • 0 kudos

Getting Started with STM32H750B-DK

I want to start writing my own code for the STM32H750 discovery board. I have installed STM32Cube IDE, MX and PROG. I have downloaded the examples for the board and I'm trying to build and run the GPIO example because its the simplest. I've chosen th...

IGeor by Associate II
  • 1327 Views
  • 0 replies
  • 0 kudos

Generating code removes my added include paths

Hi, It's my first time using STM micros and the Cube IDE.Whenever I generate code from the device configuration tool, the include paths I have added in properties > C/C++ Build > Settings > MCU GCC Compiler > Include pathsdisappear. This only happens...

JKape by Associate
  • 833 Views
  • 0 replies
  • 1 kudos

STM32F030 Erase internal flash page

Dear,I made a project for STM32F030RC with STM32CubeIDE. when I use "HAL_FLASHEx_Erase" function to erase some flash pages (at end of flash that there is no code on it) , the CPU crash. I guessed it is depended on interrupts. so I disabled interrupts...

Load symbols from more than one elf file

I have a bootloader + main application that I would like to debug. Unfortunately it looks like I can only specify 1 file to load the symbols from? In TrueStudio it was easy with the debug script file to specify more than one, but the simplified UI ...

LKory by Associate
  • 2157 Views
  • 2 replies
  • 0 kudos