STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1292 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 522 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

How do I import TrueStudio project for BlueNRG-2?

The BlueNRG-1/2 SDK provides sample projects in TrueStudio form. When I attempt to import any of them into STM32 CubeIDE, I am presented with a dialog asking for the proper MCU for the evaluation board. If there is a way to determine the correct an...

0690X00000Arj6KQAR.png
BBeau by Associate
  • 1464 Views
  • 1 replies
  • 0 kudos

STM32CubeMX file => linker script file not generated properly

Hi,I'm using STM32CubeIDE with a former Atollic TrueStudio project. The import itself succeeded, but it's neccessary to fine tune the settings. Also, when using the STM32CubeMX files, it seems that STM32CubeIDE uses different file names for several s...

RAltm by Senior
  • 3978 Views
  • 7 replies
  • 0 kudos

How to send AT Commands to HC-05 using CubeIDE ?

I am using HC-05 bluetooth module and STM32F407. I am trying to change the name of the bluetooth module. I can enter AT Command Mode, but i can't send any AT Commands to module. I tried something in main. But it didn't workHere is my try:/* Includes ...

STM32CubeIDE Code Indexer or Parser Bug

STM32CubeIDE parser or indexer not working properly. Tested CubeIDE versions are 1.0.1 and 1.1.0. Some Stm32 HAL library header files doesn't recognised as C header file and contents not accessible by IDE tools. I noticed some major issues when this ...

0690X00000ArnDeQAJ.png 0690X00000ArnGnQAJ.png
IBeRyUS by Associate
  • 1342 Views
  • 0 replies
  • 0 kudos

Upload without debugging

Hello everyone. I'm rather new to STMCubeIDE. I used a little STM Workbench in the past but never had the opportunity to work on a full project.Now, after I started a new project and worked on it, debugged it and so, I have the need to compile and up...

QcFe by Associate
  • 3671 Views
  • 4 replies
  • 3 kudos

Running debugger opens up a number of files

This is more of an observation and annoyance. Whenever I run the debugger, STM32CubeIDE (1.1.0) opens up files that I have no interest in editing. I find that I am constantly closing files in the editor while debugging my code. The files opened up ar...

Set Up IAR Toolchain in STM32CubeIde

How to configure the IAR toolchain into STM32CubeIde?, i have installed the plugin and configured the path to the installation directory of IAR and now how to configure to build a project with the IAR compiler. I don´t find where to configure it.Tha...

JSerr.6 by Associate
  • 901 Views
  • 0 replies
  • 0 kudos