STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1295 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 523 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32F429 Discovery CUBE IDE SWV printf not working

I'm using STM32F429 Discovery board and CUBE IDE. I have set the Serial Wire Debug, in debug configuration, I enabled SWV, set the core clock, enabled live expession. In main.c I wrote this part of the code int _write(int file, char *ptr, int len){  ...

Resolved! Error with auto generated drivers in CubeIDE

I am not sure this belongs here, it could just as well be in MCU, but i believe it could be a configuration problem, so i put it here.I am working on a project with Cube IDE. when I tried to compile for the first time, the build failed because of er...

Ubus99 by Associate III
  • 2160 Views
  • 1 replies
  • 0 kudos

Resolved! IDE the culprit for Hard Faults?

Hi,I'm using the F469I-DISCO Board, since a couple of days I can't pause the execution of my program, without it causing a Hard Fault after continuing. I know it doesn't have anything to do with my code, because I took old projects, which ran fine a...

STM32F429ZI UART5 data is received on terminal only for Baud rates 9600 & 4800 for higher baud rates we get garbage data. What can be the issue ?

System Clock is PLL_HSEHSE connected is 12MHzHSE_VALUE is set 12000000 & SystemCoreClock = 180000000 in system_stm32f4xx.cHCLK = 180MHzPCLK1 = 45MHzPLLM = 12;PLLN = 360;PLLP = RCC_PLLP_DIV2;PLLQ = 4;Clocks are configured as expected, cross checked RC...

Rahul1 by Associate II
  • 2983 Views
  • 7 replies
  • 0 kudos

STMCubeIDE missing FDCAN pinmux configurations for STM32H747 ?

After studying the documentation of the STM32H747 I'm pretty sure that CubeMX is missing to show at least one alternative pin muxing for the FDCAN. For FDCAN1, according to the document DS12931 Rev , it can be set for instance to PD4/PD5. But the Cu...

mkrug by Associate III
  • 1019 Views
  • 0 replies
  • 0 kudos

CubeIDE 1.1.0 import issue

Well so my first impression from CubeIDE 1.1 on Win10... looks good =)Just some issues with importing existing projects from Atollic:My Atollic projects have been imported from SW4STM, and some remnants of SW4STM still are in the .project or .cprojec...

Pavel A. by Super User
  • 1430 Views
  • 2 replies
  • 0 kudos