STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1297 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 525 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! GIT support in STM32CubeIDE

Dear colleagues,Do somebody knows whether STM32CubeIDE support GIT like any other Eclipese (Team -> Commit, Merge.... etc)?Any support is very appreciated, since I did not found any clear info in wide web.Regards,Volodymyr.

My code doesn't run without debug mode (CubeIDE)

Hi,i am using STM32CubeIDe in my project. i am using STM32F030 as transmitter and STM32F4 as a receiver. When i run my code in debug mode both of them work properly. But when i press terminate and re-insert my ST-LINK device i can't see any data in m...

Why this difference? ELF vs. binary image

Using CubeIDE 1.1 with its default toolchain.How can be explained the following mismatch between the ELF file loaded to the MCU via debugger and binary file created with objcopy? (arm-none-eabi-objcopy -O binary foo.elf foo.bin )I've read the image b...

Pavel A. by Super User
  • 1444 Views
  • 2 replies
  • 0 kudos

SPI function in STM32091C-Eval using STM32CubeIDE

Hi, I want to use SPI function from the evaluation board to connect to an FPGA. However I see that the MOSI port at pin PE15 at connector CN7 does not response. In Userguide UM1817, Table 23 said, to disconnect with function block on STM32091C-EVAL b...

CubeIDE v 1.1 - problem with SWO debug output

It looks like the CubeIDE debugger (GDB server) has issues with SWO output.When I enable SWO output in debug config and actually print something, only first few lines appear in the SWV ITM data window. Then one of following occurs:Debugger loses conn...

Pavel A. by Super User
  • 1064 Views
  • 0 replies
  • 2 kudos

Problem with nearly new Nucleo F722ZE

New Nucleo-F722ZE initially worked fine (initially prompted for software update). But after approx 3 hours when trying to Run->Debug , it now shows:Waiting for debugger connection...Debugger connectedDebugger connection lost.Shutting down...Power cyc...