SPI function in STM32091C-Eval using STM32CubeIDE
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-11-26 7:28 PM
Hi,
I want to use SPI function from the evaluation board to connect to an FPGA. However I see that the MOSI port at pin PE15 at connector CN7 does not response. In Userguide UM1817, Table 23 said, to disconnect with function block on STM32091C-EVAL board, I need to remove R83. Does this table mean that I need to remove the resistor R83, and then I can use the port? I think I got some misunderstanding here. Please enlighten me.
Thanks.
Labels:
- Labels:
-
SPI
-
STM32CubeIDE
-
STM32F0 Series
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0