STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1298 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 525 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

request: board examples using the CubeIDE project structure

When stumped, I've found that the examples in the various board zip files that STMCubeIDE downloads are very helpful. However none of them are structured in a way that I know how to load into the 'modern' STM32CubeIDE. is there any documentation aime...

mmalex by Associate II
  • 1209 Views
  • 1 replies
  • 0 kudos

Resolved! Why float X = 3300/2000 = 1?

I have a simple calculate#define VREF ((uint16_t) 3300)   float X = VREF / 2000;Why X result is 1? This happen with another calculate like xx00 / xx000Thanks

NNam.18 by Associate II
  • 2405 Views
  • 4 replies
  • 0 kudos

Can not debug on STM32CubeIDE

Failed to bind to port 61234, error code -1: No errorFailure starting GDB server: TCP port 61234 not available.​I need help:persevering_face:

CubeIDE debugger - how to control program/erase flash size?

Is this a bug in the tool or I don't understand how to tweak it?Debugging a bootlolader and app. image on a single core H743 or H753.The bootloader sits in bank1, sector 0 and the "application" in sector 1.When I begin to debug the bootloader, the de...

Pavel A. by Super User
  • 881 Views
  • 0 replies
  • 0 kudos