STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1440 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 562 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! General questions on STM32CubeIDE

Hello,(Hobbyist there) A few years ago I tried to develop on STM32 microcontrollers (the so called 'blue pill' to be exact) but the toolchain installation and the whole code generating process made me give up (also there wasn't full linux support if ...

Hi, I have a project for running on EVALKITSTKNX evaluation and development board,the project was successfully compiled by STM32CubeIDE V1.3, but there is appear a problem as below picture while execute the debug action.

 same time I try to drop the bin file to device directly, but it's still fail and feedback a message "The application file format is unknown and cannot be parsed and/or processed"Currently i can't sure what's reason caused this issue? Is it related t...

0693W000000UczbQAC.png
Roger LI by Associate II
  • 813 Views
  • 0 replies
  • 0 kudos

STM32H742 UART configure problem.

we configture the STM32 via STM32 IDE, the uart is configured to 115200 8-N-1 mode. but we receive the data via PC USB-uart. the PC tools configure to 115200 7-Space-1 mode to correct receive the data. if we configure to 115200 8-NONE-1 in PC si...

kjian.1 by Associate
  • 804 Views
  • 0 replies
  • 0 kudos

Hello I use stm32CubeIde ver 1.3.0 build 5720_20200220_1053 I'm having trouble with a new stm32 project(stm32l476rg) the first build i get error "make: ***[makefile:43 ***.elf] error 1. The error is clear to me and I know what to do.

under properties / settings I change "Floating-point unit to none but in MCU GCC Compiler in All options: the -mfloat-abi=is still 'hard'Only after many attempts the program compile success.Thankseli

Eshau by Associate
  • 813 Views
  • 0 replies
  • 0 kudos

Upgrading CubeIDE 1.2 to 1.3 fails

I could download latest HAL library for STM32L4 (which means my internet setup maybe correct), but when trying to launch an upgrade to CubeIDE 1.3, it fails (no upgrade available, server unavailable). Is it just me? (no apparent related post found so...

S.Ma by Principal
  • 2143 Views
  • 3 replies
  • 0 kudos

Is it possible to mix different amounts of colours in an RGB LED using HAL_GPIO_WritePin pinSet, as in WITHOUT using PWM?

I have a thermistor hooked up to the nucleo-l432kc to obtain temperature and display that temp on an LCD, print it to the screen, and light up a specific colour of an RGB LED. I want to be able to combine two colours of an RGB LED in different amount...

cl.1_99 by Associate II
  • 1839 Views
  • 2 replies
  • 0 kudos

Resolved! [SOLVED] How to obtain the Project name ?

There is the macro __FILE__ to know the complete path of the source code but how to estract only the project name of CubeWorkspace ?I would like to display this on my develop phase to be sure of the version running.On Arduino Due I have used this cod...

Issues importing Atollic True Studio Project

When importing my old project from True Studio to Cube IDE I get the dialog where I need to specify the processor in use (see picture).From this dialog I can not move on, no matter what i choose, one of them, all of them or none of them, or in differ...

MBohm by Associate II
  • 3618 Views
  • 5 replies
  • 0 kudos