2020-03-22 12:27 AM
There is the macro __FILE__ to know the complete path of the source code but how to estract only the project name of CubeWorkspace ?
I would like to display this on my develop phase to be sure of the version running.
On Arduino Due I have used this code but with STM32 is not easy:
void display_Running_Sketch (void)
{
String the_path = __FILE__;
String the_date = __DATE__;
String the_time = __TIME__;
String ver;
int slash_loc = the_path.lastIndexOf('\\');
String the_cpp_name = the_path.substring(slash_loc+1);
int dot_loc = the_cpp_name.lastIndexOf('.');
String the_sketchname = the_cpp_name.substring(0, dot_loc);
ver = the_sketchname + " " + the_date + " " + the_time;
myGLCD.setFont((unsigned char *)SmallFont);
myGLCD.setColor(255, 255, 255);
myGLCD.print((const char *)ver.c_str(), CENTER, 1);
delay(1000);
myGLCD.print((char *)" ", CENTER, 1);
}
Solved! Go to Solution.
2020-03-22 2:14 AM
The Eclipse IDE (on which CubeIDE is based) has a predefined macro ${ProjName} that you can assign to a C macro.
Navigate to
Project / Properties / C/C++ Build / Settings / Tool Settings / MCU GCC Compiler / Preprocessor
Set the Configuration line at the top to [ All configurations ]
Use the green + symbol next to Define symbols (-D) and enter
PROJECTNAME="${ProjName}"Now you can use the PROJECTNAME macro as a string value in your project.
2020-03-22 2:14 AM
The Eclipse IDE (on which CubeIDE is based) has a predefined macro ${ProjName} that you can assign to a C macro.
Navigate to
Project / Properties / C/C++ Build / Settings / Tool Settings / MCU GCC Compiler / Preprocessor
Set the Configuration line at the top to [ All configurations ]
Use the green + symbol next to Define symbols (-D) and enter
PROJECTNAME="${ProjName}"Now you can use the PROJECTNAME macro as a string value in your project.
2020-03-22 3:43 AM
Very good, thank you
void LCD_LOG_Ver2()
{
BSP_LCD_SetFont (&LCD_LOG_TEXT_FONT);
BSP_LCD_SetTextColor(LCD_LOG_TEXT_COLOR);
BSP_LCD_DisplayStringAt(5, 5, (uint8_t *)PROJECTNAME, CENTER_MODE);
}