STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1440 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 564 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

CubeIDE Rendering issues on Linux (SOLVED)

I have some annoying rendering issuse with CubeIDE 1.3 running on Ubuntu 19.10 (Pop_OS).The problem is that some of the toolbox windows are not updating/re-rendering when switching tabs or perspective.Debug perspective seems to have most issues, see ...

Blem.1 by Associate
  • 1715 Views
  • 1 replies
  • 0 kudos

Resolved! how to setup clock when STM32CubeIDE empty project is used?

hi All.My name is Alfredo, I just have got a Blue_Pill_STM32F103C8 board.I just installed STM32CubeIDE (Version: 1.3.0), i wrote a small project as toggle led using the CubeIDE configuration and everything is fine. but now i am trying to do the same ...

ERABALF by Associate III
  • 4721 Views
  • 4 replies
  • 1 kudos

Error in my cube ide code (Using Mat-target)

I get an error everytime i try to debug LED2. The error says: expectet identifier or `(` before `{`token. I added a screenshot of the code and where exactly the error is positioned. The code was modeled by simulink

Driko by Associate II
  • 2978 Views
  • 3 replies
  • 0 kudos

STM32CubeIDE FreeRtos USB

Hi,I have problem with automatick generated code from STM32CubeIDESTM32CubeMX: 5.6.0MCU: STM32F407FreeRTOS API CMSIS v2I have two problems (at least)I have to change macro in usbh_conf.h, after this alloc works.#define USBH_malloc malloc #def...

JSvat.1 by Associate
  • 937 Views
  • 0 replies
  • 0 kudos

Resolved! Cant generate code, because CubeIDE didn't find firmware in /STM32Cube/Repository/ which was automatically downloaded installed

Fresh installation, when I try to create a STM32 project a zip file with firmware is downloaded and unpacked, but I still get this error message:"Code generation could not be done because necessary firmware package is missing. Not able to complete ST...

0690X00000DBD3lQAH.png
KOlsz.1 by Associate II
  • 13286 Views
  • 3 replies
  • 0 kudos

Win10 - make permission denied

Hello, i installed on company laptop STM32CubeIDE to default folder C:/ST/... and created the workspace under c:/users/<username>/... by rightclick on installer --> execute as Admin.Afterwards I created a new project and tried to build, but then I g...

DBuet.1 by Associate
  • 914 Views
  • 0 replies
  • 0 kudos

How to force include path update ?

Hello,I use STMCube IDE v1.3.0 Build: 5720_20200220_1053 (UTC)When building, the include path are not updated with the include path properties.I notice this mis-alignement is caused in the cproject :include path are correct here : <option IS_B...

FTouq.1 by Associate II
  • 4312 Views
  • 6 replies
  • 0 kudos

Debug Configuration

HelloDebug Cofiguration-Debugger-Reset behaviorThere are None, Software system reset, Connect under resetPlease explain each behavior.If you select Software system reset or Connect under reset, an error may occur.Thank you.

Ebun.1 by Senior
  • 4224 Views
  • 4 replies
  • 3 kudos