STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1415 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 558 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

I ordered Nucleo-L4A6ZG few days ago, but CubeIDE 1.4 doesn't support Nucleo-L4A6ZG. How can I develop my board?

I ordered Nucleo-L4A6ZG few days ago, but CubeIDE 1.4 doesn't support Nucleo-L4A6ZG. ​I don't have enough time to wait for a new order, I have to develop my board until next week. ​Is there any solution to develop Nucleo-L4A6ZG board with STM32cubeID...

SLEE.5 by Associate
  • 1276 Views
  • 3 replies
  • 0 kudos

Can't debug NUCLEO-F746ZG in STM32CubeIDE

Hi AllI can drag and drop a binary file to the NUCLEO-F746ZG via its mbed hard drive that appears when the board is connected to the PC and the program runs.I can also try to debug from STM32CubeIDE and it successfully programs and verifies the code ...

hpipon957 by Associate III
  • 4391 Views
  • 9 replies
  • 0 kudos

Resolved! How to store compilation date in the final binary file in order to read it by an external program?

I am trying to migrate a project from IAR to STM32CubeIDE. In this project, I have two lines of code in the main (as global variables) that store the compilation date in the final binary file. These two lines are the following:char const compilation_...

Resolved! How to download and use STM32 Standard Peripheral Libraries (for example: stm32f10x_rcc) instead HAL libraries?

Hello,When I create a new project in STM32CubeIDE, automatically it downloads all HAL libraries (for examples: stm32f1xx_hal_rcc or stm32f1xx_hal_tim) but I want to use the STM32 Standard Peripheral Libraries (for example: stm32f10x_rcc or stm32f10x...

CubeIDE project export to CMake ?

It is not a secret that lot of people dislike Eclipse. At very least, it is heavy and complicated for young students.Also it is understandable that ST has invested in CubeIDE heavily, and CubeMX is Java-based, and True Studio is well alive.So here is...

Pavel A. by Super User
  • 1686 Views
  • 0 replies
  • 4 kudos

Source file accessible through static library. How to disable?

I need to share some code to third party in static library form such that my source code won't be accessible to them.I was able to create a static library project using STM32CubeIDE's New project > Static library option.The project compiled successfu...

SShid by Associate III
  • 901 Views
  • 0 replies
  • 0 kudos

What limits stack size?

Hello I am working on STM32L072 series MCU. I am using Stm32cubeideMy project is using %94 of RAM. I need more stack on my project. I tried to increase stack in linker file, but i get error. I think, there is enough area in my ram. Additionally, I ca...

CYesi.1 by Associate II
  • 5275 Views
  • 4 replies
  • 0 kudos