STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1093 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 476 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

I will try to ping another ip with STM32F207VG.

I pinged STM32 with my PC.However, STM32 did not find a way to ping another ip.Ask for advice.I am using STM32F207.I'm using STM32CubeIDE.I am using FreeRTOS.I called functions in api_lib.c to connect the network.The PC pinged STM32 and the response ...

Lyoun.1 by Associate
  • 762 Views
  • 0 replies
  • 0 kudos

Resolved! Debugging .hex file on STM32f469i Board

Hello All,I want to load AND debug a precompiled .hex file onto my STM32f469i Discovery board. I've looked around and tried several tools such as the STM32CubeIDE and the ST-Link utility, but no luck. The CubeIDE seems to be unable to flash the file,...

TLian.11 by Associate II
  • 5760 Views
  • 10 replies
  • 0 kudos

SWV Exception Trace is not working in STM32CubeIDE

I want to trace exceptions/interrupts happening in my board with STM32L4xx in STM32CubeIDE by `SWV Exception Trace Log` and `SWV Trace Log`. I use SEGGER J-Link and In Debugger I have correctly set the interface to SWD and the Core Clock to 80 MHz. A...

KK.1 by Associate
  • 1031 Views
  • 0 replies
  • 1 kudos

unknown type name '_ARMABI'

Hi Sir,I'm transferring code from Keil to CubeIDE. During compilation, i cannot find the way to solve the error unknown type name '_ARMABI'. _ARMABI is defined in many header files including stdio.h and time.h in Keil environment, but I cannot find w...

LChan.5 by Associate II
  • 1098 Views
  • 1 replies
  • 0 kudos

Is there an example of smbus master and slave usage ?

I am trying to use smbus to talk to a charger chip. Is there any example on how this works ?I am using the following HAL API.HAL_SMBUS_Master_Receive_IT(&hsmbus1, 0x0b, &reg_val[0], sizeof(reg_val), SMBUS_FIRST_AND_LAST_FRAME_NO_PEC);IRQ handler:void...

PRedd.111 by Associate III
  • 1499 Views
  • 1 replies
  • 0 kudos