Hi, I find that there is no "download" button in the stm32cubeide. If users want to download the codes which generated by stm32cubeide(stm32cubemx), they must click the "debug" button first, then the software goto the UI of debug, and then the code d...
Hi, I installed STM32CubeIDE for the first time. As the picture illustrated, the keywords, GPIO_PinState and uint32_t, seems like the comment, is there anyway to solve this problem?Best regards.
Posted on September 03, 2016 at 15:52
Hi, i'm studying stm32f407, but there is a problem puzzling methose days. It's about the WWDG.
I just want to test the function of WWDG, so in my function which has been wrote to initialize the WWDG, i...
Hi, Andy, I didn't explain it clearly, it's my fault.The comment is light Green, GPIO_PinState and uint32_t is a little dark Green to me. They're all green, so it's not easy to distinguish them.