STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1671 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 627 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Add a .lib library to a project

I have a .lib file created using KeiluV5 and would like to use it in a CubeIDE project. How do I go about doing this?I have found reference to Libraries and Library Paths at Project > C/C++ General > Paths and SymbolsI've tried adding my .lib file a...

Correctly include external files (.c and .h)

Hello,I am new with STM32CUBE. I have a weather station that I want to couple on the STM32F411 PCB (from Aliexpress). It works when I put the uint8_t WH24P_Data[21] data buffer in main.c. I have made WH24P.c and WH24P.h and I want to declare this buf...

Avan .4 by Associate
  • 7010 Views
  • 4 replies
  • 0 kudos

Resolved! 1.4.0 regression: can no longer debug through ftdi (ft4232h) with openocd, saying "No ST-Link detected"

I've been debugging a custom designed board that has an FT4232 USB IC on it with a JTAG interface. STM32Cube IDE up to 1.3.1 could successfully debug this through openocd. Version 1.4.0 wants to force firmware verification so I can no longer program ...

dawid by Associate III
  • 6127 Views
  • 13 replies
  • 0 kudos

STM32F407 Debugger Lost Connection Cube IDE V1.4

Hi ST community,I am using STM32 Discovery board STM32F407 DISCO, I have written a Simple toggle Code, Compile and build has no errors, but when i run the code the error is throwing called "Debugger Lost Connection, Waiting for Connection", PFA imag...

0693W000003BtXdQAK.png
AShiv.437 by Associate II
  • 1660 Views
  • 2 replies
  • 0 kudos

Resolved! How to change starting address of my project

I'm currently using a STM32F030CC and i need a Bootloader and Main App structure. The problem is that i can't find in system_stm32f0xx.c constant VECT_TAB_OFFSET to change. Also SCB->VTOR is missing. I'm currently using SMT32CUBEIDE v1.4.1. Any ideea...

BAlex.3 by Associate
  • 2700 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.