2020-02-19 7:59 AM
Hi,
I am attempting to use the example code from CMSIS documentation here: https://www.keil.com/pack/doc/CMSIS/RTOS2/html/group__CMSIS__RTOS__Wait.html\
But it results in HardFault.
Working around currently by using
#include "FreeRTOS.h"
#include "task.h"
and running the bare FreeRTOS syntax and functions:
void StartLedBlink01(void *argument)
{
/* USER CODE BEGIN 5 */
TickType_t lastWakeTime;
const TickType_t frequency=500;
lastWakeTime=xTaskGetTickCount();
/* Infinite loop */
for(;;)
{
vTaskDelayUntil(&lastWakeTime,frequency);
HAL_GPIO_TogglePin(LD2_GPIO_Port, LD2_Pin);
}
// Add termination if exit the loop accidentally
osThreadTerminate(NULL);
/* USER CODE END 5 */
}
Is there any way to make the CMSIS osDelayUntil() function work properly?
The osDelay() function works fine, but I need the functionality of the osDelayUntil function.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.