User Activity

I'm failing to get the indexer working correctly.So far I've tried several solutions regarding paths definition and Eclipse memory sizes allocation. All of them leading to the same error for all the files in my project. See an extract of the .log fil...
Hello,I'm working on a USB MIDI device and I'm facing an issue with Mac computers: when the host goes to sleep, it keeps sending SOF (start of frame) messages. Thus, there's still activity on the bus preventing the STM32 to turn to Suspend mode.Then,...
When running my application from the debug session for CM7 (CPU1), the CM4 (CPU2) isn't detected as being in "Stop Mode", which leads to a timeout and therefore an error detection.If the debug session is stopped, the application runs as expected afte...
Kudos from