STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1427 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 558 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Stop console output for Live Expressions

Hello,Using LiveExpressions produces a large amount of unwanted console output like "Reading x bytes @ address 0xxxxxxxxx".Is it possible to disable such console output when not needed?Thank you in advance.

Resolved! Triggering ADC/DMA with Timer2 (STM32WB55)

Hello! I had a project where I'm trying to get the ADC/DMA to trigger with timer 2 but I seem to be missing part of the puzzle to getting it up and working. I originally had the ADC/DMA running with "Continuous Conversion" mode set in the ADC, which ...

0693W000003RMCZQA4.jpg 0693W000003RMCUQA4.jpg 0693W000003RMCAQA4.jpg 0693W000003RMC0QAO.jpg
JayDev by Senior II
  • 2055 Views
  • 1 replies
  • 0 kudos

How do I add an MCU target to an imported CMake project?

I've inherited an existing project. It's got STM HAL / auto-generated code. It's set up with CMake to be compiled at the command line. I've imported it into STM32CubeIDE and it builds.I have an STM32F407G-DISC1 board (MB997D). Using a hack, I've mana...

SMacD.1 by Associate II
  • 1969 Views
  • 2 replies
  • 0 kudos

STM32F74XX I2C Fast-Mode Plus Configuration

According to the the STM32F74XXX Reference Manual, the STM32F74XX supports Fast-mode Plus I2C (up to 1MHz).I have configured my application's I2C to Fast-Mode Plus through STM32CubeIDE tools but I get the following error during build time: undefined ...

LMend.1 by Associate II
  • 2184 Views
  • 3 replies
  • 0 kudos

Resolved! Hi. My version of IDE is 1.4. My board is NUCLEO F-446RE. I've updated ST-LINK firmware without mass storage (as was proposed in another topic). Yes, I've read many other related topics but ... nothing helped. PLEASE help I'm absolutely stuck!

Here is what I get:STMicroelectronics ST-LINK GDB server. Version 5.6.0Copyright (c) 2020, STMicroelectronics. All rights reserved.Starting server with the following options:    Persistent Mode      : Disabled    Logging Level       : 1    Listen Por...

OSamu.1 by Associate II
  • 2857 Views
  • 9 replies
  • 0 kudos

What software to program STM32L4 device ?

Hello everyone, I recently bought a Nucleo-L4 board and I wanted to program it with CubeIDE on windows. The matter is each time I run the installer I have "NSIS error" telling me that it can run the installer. What other software do advice me to use ...

Mc3 by Associate II
  • 1676 Views
  • 2 replies
  • 0 kudos