STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1440 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 562 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

[STM32H743I-EVAL2] Debug inquiry

I am testing with STemWin demo program on STM32H743I-EVAL2.​Other applications program work well with the debugger on STM32H743I-EVAL2.​But the STemWin demo program only the debugger doesn't work.​What's the problem?​STM32CubeIDE Version: 1.4.0​​STM...

0693W000004GeYVQA0.png
KSang.2 by Associate
  • 782 Views
  • 0 replies
  • 0 kudos

About a folder that is made by stmcube id itself .

Hello , I am using stmcubeide for my project but due to some reasons i have deleted that project folder . Now when i am opening the cubeide it makes that folder itself and when i open that it shows errror . when i delete that folder and open the cube...

KJangu.2 by Associate II
  • 1603 Views
  • 0 replies
  • 0 kudos

Debug using STM32CubeIde ??

Hello, I am working on a card with an STM32H745 processor.I have a few questions regarding debugging (with a V3 probe):1) is it possible to make a hard reset of the chip?2) is it possible to reset the cores independently?3) is it possible to do some ...

JVERN.18 by Associate III
  • 2528 Views
  • 3 replies
  • 0 kudos

Nucleo-F446ZE Error in final launch -- see attachment. First time I hooked it up. Configured with CubeMX and started a debug session in CubeIDE without making any changes to code and received this error. No idea where to start correcting it.

I'm new to STM32 products and have been working with the Nucleo-G474RE. Everything has been working well. Switched over to the new Nucleo-F446ZE and receive this error. Switched back to G474 and every thing works fine. Any idea what is happening a...

DIngr.1 by Associate II
  • 906 Views
  • 0 replies
  • 0 kudos

Resolved! Build project encounters problem

Hi !There is an error while building project as shown in the picture below and more error details are like :"Errors occurred during the build.Errors running builder 'CDT Builder' on project 'STM32F072CBU_CDC_STM32_CUBE_IDE'.java.lang.NullPointerExce...

Resolved! How to set --fdebug-prefix-map in the STM32CubeIDE

Hi,I'm building my project inside a Docker container that has STM32CubeIDE installed using the command:headless-build.sh -build demo-nucleo-f334r8 -importAll /appThe project builds fine, and I'm able to successfully flash my board with the generated ...

ADhan.1 by Associate II
  • 2272 Views
  • 1 replies
  • 0 kudos