Skip to main content
KVeer.1
Associate
Apr 8, 2020 3:53 PM UTC
Question

STM32F446RE lost connection with debugger suddenly while previously working (STM32Cube IDE running on Linux)

Hello all,

I am using a STM32F446RE and am programming it using STM32Cube IDE. I am running it on Linux 18.04 LTS. It was perfectly working previously and now suddenly dont know what happened, it prompts the following message when I am connecting to the debugger. I didnt mess with the board or the the debugger settings on my PC.

The console prompts the following:

STMicroelectronics ST-LINK GDB server. Version 5.5.0

Copyright (c) 2019, STMicroelectronics. All rights reserved.

Starting server with the following options:

       Persistent Mode           : Disabled

       Logging Level             : 1

       Listen Port Number        : 61234

       Status Refresh Delay      : 15s

       Verbose Mode              : Disabled

       SWD Debug                 : Enabled

       InitWhile                 : Enabled

Waiting for debugger connection...

Debugger connected

Debugger connection lost.

Shutting down...

I also saw these under my debug window. Not really sure what this means.

0693W000000VYtvQAG.png

Could anyone kindly tell me what I could do? Any help would be greatly appreciated!

[edit]

I had a backup board and connected it to the PC and tried a debug session and it worked! Do you guys think that the controller might have been zapped somehow?

This topic has been closed for replies.