STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1493 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 571 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

how to use a string (class) in ST32 Cpp code

hello everyoneI'm trying to use a string type (string class not char pointer or array) in my codeI have a lot of string messages in my program and a string class can help a lotI see how arduino did it in their IDE, their string class is good, I think...

MBany.1 by Associate
  • 5736 Views
  • 1 replies
  • 1 kudos

Resolved! What is required to utilize USART3 on the STMod+ Fan-Out Expansion Board when using the STM32L4P5G-DK Discovery Kit?

I start a new project with the following steps:I create a new STM32 ProjectI select STM32L4P5G-DK from the Board Selector MenuI initialize the board with it's default configurationI have successfully configured the I2C4 and USART2 peripherals on the ...

0693W000005Ag24QAC.png 0693W000005Ag2EQAS.png
Zak by Associate II
  • 2103 Views
  • 3 replies
  • 0 kudos

PWM Combined 3 Phase Mode, ADC Trigger Problem

Hey,1- I started 6 PWM Complementary mode and also added Channel 5 No output to trigger interrupt using it.2 -Interrupt called TIM1_TRG_COM_TIM17_IRQHandler3-There no running on interrupt I put a LED in interrupt but no action.So my all settings foll...

EDuat.1 by Associate III
  • 767 Views
  • 0 replies
  • 0 kudos

Debugging in STM32CubeIDE

Hello,I am working on a project where I have created several of my own files (.h and .cpp) but I am having issues with undefined reference to certain functions. I cannot solve this issue while having the files separated, but I was wondering if it is ...

MCrew.1 by Associate III
  • 2701 Views
  • 4 replies
  • 0 kudos

Problem mounting SDCard on STM32h745 using HAL

Hi, I'm having some issues mounting my SDCARD on my board. I'm trying to write data to the SD card using SDIO 4-Wire and I'm using a STM32h745 Nucleo board with a Waveshare Adapter but so far, I've been unsuccessful in getting the SD card initialised...

JArap.1 by Associate
  • 843 Views
  • 0 replies
  • 0 kudos

Nucleo-F070RB USB HID mouse not enumerating

Hi,I'm trying to get the example from the stm32 USB traing video https://www.youtube.com/watch?v=6MJJwDKsKsc&t=884s to work using STM32CubeIDE and the Nucleo-F070RB dev board.Everything compiles fine and I get no error when running it, but I can't ge...

MHamb.1 by Associate
  • 1333 Views
  • 1 replies
  • 1 kudos

Variable Substitution in Debug Configuration

In Codewarrior 11.x under the debug configuration C/C++ Application section I can enter "${BuildLocation}/PE-15B00.elf" and that debug configuration is used for all my different build configurations. In STM32CubeIDE, when I try to use variables in ...