STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1488 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 571 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32Cube should generate clock defines

Hi,I want to know the configured core clock frequency at compile time, but unfortunately this value is not defined anywhere. Thus I propose that the code generator should create a list of #defines for every node in the clock tree. I think SYSCLK, HCL...

jirre.1 by Associate II
  • 2002 Views
  • 2 replies
  • 1 kudos

Stm3210C- Eval CAN1 not working (Hard Fault)

I have been wanting to use Hal_CAN library and everytime I use HAL_CAN_AddTxMessage using cube IDE I get an Hard fault. So if anyone has a good CAN bus transmission and recieve Example that would be really helpful.

ASing.11 by Associate II
  • 2549 Views
  • 5 replies
  • 0 kudos

how can I manage my code with cubeIDE

I'm a beginner using stm32 and cubeIDE. I find that having all the setup and functions in one file is a little annoying to navigate - is there a way I can put my functions in a different file, for example? Or what are some way of managing large progr...

deep_rune by Associate III
  • 2314 Views
  • 4 replies
  • 0 kudos

Difference between STM32CubeIDE and KEIL

I'm using STM32F103RB with I2C to access BMP280. WIth KEIL the program worked well,But with STM32cubeIDE I got the I2C bus busy always. Could anyone tell me what is wrong?The projects files are attched.

DDong.2 by Associate II
  • 897 Views
  • 0 replies
  • 0 kudos

Hi guys, unfortunately, I did something that I can not spot in my project and it is not compiling anymore. cubmixIDE is saying that: "undefined reference to `HAL_UART_Transmit'" anytime I'm using `HAL_UART_Transmit'.

as people told me, i looked on "makefile" vs last version "makefile" to see any change but i couldnt spot one.I did all necessary "#incuded" on top of the class.I'v attached the problematic part:#include "main.h" #include <string.h> #include <stdboo...

Gbasi.1 by Associate II
  • 1642 Views
  • 3 replies
  • 0 kudos