STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1437 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 560 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Excessive extra projects being imported with new Cube

A couple of weeks ago STM32Cube disappeared off my computer. I went a got the install file for the most recent version (2.1.1). Since I have installed this when I try to import an old project into the workspace or use MX to generate code when trying ...

GTann1_0-1777535558488.png GTann1_1-1777535598806.png
GTann.1 by Associate III
  • 150 Views
  • 3 replies
  • 2 kudos

Install CubeIDE on Raspberry Pi 5

Has anyone had success installing the Cube IDE on a Raspberry Pi 5?  I first got the error message "Installation dir cannot be temporary one: /home/my_name/Downloads/makeself_dir_o70WRx"I tried various workarounds suggested by Gemini, ultimately crea...

Resolved! IDE 1.15.1 login error on Windows 11

STM32CubeIDE 1.15.1 login error, although Check Connection shows "green" in the "Firmware Updater". Because of the Login error I cannot Install "STM32CubeU0 Firmware Package V1.0.0 / 12-February-2024". I have seen in the Forum, that this kind of erro...

miga by Associate II
  • 3142 Views
  • 10 replies
  • 0 kudos

Regarding the use of DMA to transfer ADC data

Hello everyone, I recently encountered a strange BUG.I use DMA to transfer ADC data. Previously, this program was configured this way without any problem, but it suddenly doesn't work these two days. What's even stranger is that I used STlink in the ...

CubeIDE: show version of the IDE

Dear ST Team,I use multiple versions of CubeIDE and would appreciate it if the currently running IDE version could be displayed in the following screens (somewhere).Thank youLike its done in GfxDesigner  

cubeIDE version 0.png cubeIDE version 1.png cubeIDE version 2.png ferro_1-1777656051778.png
ferro by Lead
  • 392 Views
  • 13 replies
  • 8 kudos