STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1548 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 587 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

protected files change

I use cubeIDE 1.5.1. I download standart example BLE_HeartRateFreeRTOS. It has got file app_conf.h In cubeIDE it has got strange icon. In app_conf.h I change CFG_LED_SUPPORTED to 1 and save. Clean and Build. But app_entry.c still thinks that define i...

0693W000006HwDLQA0.png

Resolved! undefined reference to

Hello!Can somebody say what im doing wrongI have project in STM32CubeIDE with lwip and freertosIm trying to add new thread(as new task) with exist principles and cant do it/* Definitions for TCPip */osThreadId_t mtcpConHandle;const osThreadAttr_t mtc...

Agde.1 by Associate III
  • 5251 Views
  • 9 replies
  • 0 kudos

Resolved! Distribuited compilation.

Hi,due to size of project, i would like to know if there is some plugin to distribuite compilation over more cores like Incredibuild does on visual studio or is it possible, meaning it is supported to develop for stm32 under visual studio.Even other ...

FMarr.2 by Associate III
  • 1610 Views
  • 2 replies
  • 1 kudos

Resolved! How to use STM32F407 FSMC memory ?

Hi,I'm working in a project that contains large data need to be processed by using stm32f407 Disc1. I facing issue with RAM overflow so, I need to use external ram by using FSMC.what is the large size of external ram that I can use it? , Is this exte...

MHass.2 by Associate III
  • 2353 Views
  • 1 replies
  • 0 kudos

Resolved! CubeIDE is unable to install the v1.6.1 update on macOS

This is less of a question and more of a statement for your information. I was not able to install the v1.6.0 update and have just been ignoring the notifications for a while, so when I saw that v1.6.1 was available I thought I'd try that but it stil...

Resolved! Empty folder required to keep project structure

On a dual core project created with the configuration tool(STM32CubeIDE Version: 1.6.0) in the IDE project explorer there is a folder with path: /LedFlash1_CM7/DriversLocation: C:\folderA\flolderb\LedFlash1\CM7\DriversThis IDE folder only contains Li...

DUgbo.1 by Associate II
  • 2644 Views
  • 4 replies
  • 0 kudos

�?CubeIDE】Why delete my Src folder ?Why haven't you fix it for so long?

Sorry,I really want to curse the CubeIDE/CubeMX development team�?�?�?�?�?�?�?Because of you, the results of my work are gone three times�?�?�?�?Not Once,Not Twice ,It is Three,Three,Three�?�?�?�?�?�?​For the first time, I thought I deleted it by mis...

abbb.12 by Associate II
  • 8419 Views
  • 17 replies
  • 4 kudos