STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1548 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 587 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

stm32cubeide error: debuger connection lost, how to solve it?

Excuse me!When I used STM32CUBEIDE to run the code, when I add the code in the red box as shown in picture, there existed a problem: debugger connection lost, when I wanna debug, the program runs into the " Hard fault interrupt"function. If I delete ...

0693W00000AOeKJQA1.png 0693W00000AOeJzQAL.png
1123.2 by Associate
  • 1587 Views
  • 2 replies
  • 0 kudos

CLEAN PROJECT

make: *** No rule to make target 'clean'. Stop. How can I fix this error in STM32CUBEIDE?

STayl.3 by Associate II
  • 1516 Views
  • 1 replies
  • 0 kudos

MPLAB features available in CubeIDE?

Hello.In MPLAB IDE there are two features that I find very helpful. (please see the attached file)Feature 1: Call GraphFeature 2: The code flow of where the cursor isAre any of these features available in CubeIDE?(Sorry I had to blacken things out, t...

mTiet.1 by Associate
  • 1851 Views
  • 2 replies
  • 0 kudos