STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1548 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 587 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

cubeide freezing

Hi,I have two functions that set visible and invisible some boxes on the same screen. When I debug the main.c and change the variable to call functions, half of the screen invalidates and sometimes, debugging freezes somewhere. Every time it freezes ...

Ezgi by Senior
  • 993 Views
  • 1 replies
  • 0 kudos

Resolved! Hi I am beginning using STM32CUbe IDE and I ant to migrate a Keil uBision project where I have a code calling two ASM functions.

these are the functions__asm void my_strcpy(const char *src, char *dst){loop   LDRB r2, [r0] ; Load byte into r2 from memory pointed to by r0 (src pointer) ADDS r0, #1 ; Increment src pointer   STRB r2, [r1] ; Store byte in r2 into memory pointed ...

HMero.1 by Associate II
  • 2599 Views
  • 4 replies
  • 0 kudos

CubeIDE is very slow after the update

After upgrading to the new version of CubeIDE (Version: 1.6.1), the change between two .ioc configuration cards takes about two minutes. Could you please speed it up?

FVese.1 by Associate
  • 3124 Views
  • 4 replies
  • 0 kudos

Resolved! STM32F479VI no SDRAM in CubeiDE?

HiI just testing some options for a future project which possibly involves a STM32F479VIT and I try to understand if it can handle an IS42S16400J-7TL SDRAM module.So I created a test project in CubeIDE but it does not show any SDRAM option in the FMC...

0693W00000AOo0OQAT.png
PGroe.2 by Associate III
  • 1732 Views
  • 2 replies
  • 0 kudos

stm32cubeIDE use 90% cpu for java in linux(ubuntu) !

hii use of stm32cubeIDE ver 1.6.0cpu core i7 6700k ram 16 GBos linux (ubuntu 20.04.2 LTS) 64bitmemory ssd 250 GB samsung-----Most of the time when using the software, after a few minutes of use, the Java usage of the CPU reaches 90% or higher and the...

kshin.111 by Associate III
  • 2286 Views
  • 3 replies
  • 0 kudos

Thread awareness debugging in FreeRTOS [STM32CubeIDE 1.1.0 has a bug for using "-rtos FreeRTOS" on ST-LINK(OpenOCD)].

In STM32CubeIDE 1.0.2, after I added '-c "$_TARGETNAME configure -rtos FreeRTOS"' to 'OpenOCD Options', I could debug FreeRTOS's target with threading mode.But, in STM32CubeIDE 1.1.0, even if I set same settings to 'OpenOCD Options', I could not debu...

Resolved! How to add new flag to build a extra library

HelloI am a beginner. I am trying to build my project using the minmea library but I got a "timegm" warning.In the library page says <Some systems lack timegm. On these systems, the recommended course of action is to build with -Dtimegm=mktime which ...

A..1 by Associate II
  • 3355 Views
  • 2 replies
  • 0 kudos