Hi I am beginning using STM32CUbe IDE and I ant to migrate a Keil uBision project where I have a code calling two ASM functions.
these are the functions
__asm void my_strcpy(const char *src, char *dst)
{
loop
LDRB r2, [r0] ; Load byte into r2 from memory pointed to by r0 (src pointer)
ADDS r0, #1 ; Increment src pointer
STRB r2, [r1] ; Store byte in r2 into memory pointed to by (dst pointer)
ADDS r1, #1 ; Increment dst pointer
CMP r2, #0 ; Was the byte 0?
BNE loop ; If not, repeat the loop
BX lr ; Else return from subroutine
}
__asm void my_capitalize(char *str)
{
cap_loop
LDRB r1, [r0] ; Load byte into r1 from memory pointed to by r0 (str pointer)
CMP r1, #'a'-1 ; compare it with the character before 'a'
BLS cap_skip ; If byte is lower or same, then skip this byte
CMP r1, #'z' ; Compare it with the 'z' character
BHI cap_skip ; If it is higher, then skip this byte
SUBS r1,#32 ; Else subtract out difference to capitalize it
STRB r1, [r0] ; Store the capitalized byte back in memory
cap_skip
ADDS r0, r0, #1 ; Increment str pointer
CMP r1, #0 ; Was the byte 0?
BNE cap_loop ; If not, repeat the loop
BX lr ; Else return from subroutine
}
The GNU compiler doesnt accept these functions
Please can you tell how to change these functions?
Best regards and thanks in advance
Horacio Merovich