User Activity

I am using STM32CubeIDE version 1.17.0 and trying to develop a custom board using X-CUBE-DISPLAY with a graphics display using the ST7789V controller.  This is a design update for a previous board that was using a 7-segment LCD display.  I have a pre...
Continuing saga of attempting to run a TouchGFX demo on a NUCLEO-G071RB with X-NUCLEO-GFX01M2($AZ2).I connected the NUCLEO board, selected it in TouchGFXDesigner, then selected the relevant demo.Having installed the latest TouchGFXDesigner (4.24.2), ...
1.I have TouchGFX Designer 4.24.2 and STM32CubeMX running on Windows 11.  I downloaded the demos and examples via the file menu, also the latest TouchGFX Generator via CubeMX.  I am targetting a NUCLE0 STM32G071 with GFX01M2($AZ2) display, so I selec...
I have a NUCLEO -G071RB board with an X-NUCLEO-GFX01M2 display shield, and am trying to run the X-CUBE-DISPLAY demonstration software GFX01M2_HelloWorld.  I have imported the project to CubeIDE and built it OK, but when I try to run it I get an error...
Having upgraded CubeIDE to version 1.17.0 using 'check for updates' and found it didn't work for my project, I tried to go back to version 1.15.1 using the revert button.  After running this, the IDE would not start and give an error message indicati...
Kudos from