STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1549 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 588 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! I just upgraded my IDE to 1.9.0. I am trying to get Segger JLink to work in debug mode. It is able to connect and download the firmware to the MCU but it shuts down straightaway after doing so. How do I stop it from shutting down? It didn't do that 1.6.x.

SEGGER J-Link GDB Server V7.62a Command Line VersionJLinkARM.dll V7.62a (DLL compiled Feb 23 2022 17:02:35)Command line: -port 2331 -s -device STM32L4Q5RG -endian little -speed 4000 -if swd -swoport 2332 -vd-----GDB Server start settings-----GDBInit ...

EAng.1 by Associate II
  • 2926 Views
  • 5 replies
  • 0 kudos

Problem with "Symbolics loading was requested but the file was not specified or not found" when uploading debugger info to board

I have a nasty problem with my STM32 Cube IDE on one machine. I had moved the working folder using the Export from STM32 CubeIDE in one machine to another where I used the import tool as I followed the info from STM on the web on how to do this. Alt...

0693W00000D1mvsQAB.png
CBarb.1 by Associate III
  • 7350 Views
  • 11 replies
  • 0 kudos

Build configurations setup

Hi,I am using STM32CubeIDE to develop our project over a stm32l4x controller. I have different build configurations, and I would like to know if it is possible to define a different output file name for each build configuration.Best regards and thank...

Angel1 by Associate II
  • 4203 Views
  • 5 replies
  • 0 kudos

Why does this simple for loop cause run time faults?

I have made a for loop that produces the data of a sine wave and stores the values in an array. The loop is set to execute in the main(). However this seems to break whatever board i use, i have tested on L47RG and the H745i. Any help would be apprec...

AHnat.1 by Associate
  • 1381 Views
  • 4 replies
  • 0 kudos

Can not find -l-l Error in STM32CubeIDE

I'm using STM32-NucleoL053R8 board. I'm Getting error when I build my project I have included required libraries and its path to the project still getting error. I tried with the manual method like adding lib to the "MotionAC2_CM0P_wc32_ot.a" file ad...

0693W00000LwP9mQAF.png 0693W00000LwPB9QAN.png 0693W00000LwPBOQA3.png
VB.4 by Associate II
  • 2721 Views
  • 4 replies
  • 0 kudos