cancel
Showing results for 
Search instead for 
Did you mean: 

Can't install package in Embedded Software Packages Manager (M1 Pro)

KFeng.2
Associate

Environment:

  • STM32Cube IDE version 1.8.0/1.9.0
  • MacBook Pro 14" 2021 (Apple M1 Pro / macOS Monterey 12.3)

To reproduce:

  • Help > Manage Embedded Software Packages
  • Can't select any items to install
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Florent V
ST Employee

Hi @KFeng.2​ ,

Indeed it is a known bug on MacOS.

Waiting for a fix, there are 2 workarounds:

  • Download the pack manually and install it using "From Local..." button from "Embedded Software Packages Manager" window. Or
  • If the project has been created through CubeMX standalone, you can install the pack from CubeMX.

Regards,

Florent

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
Florent V
ST Employee

Hi @KFeng.2​ ,

Indeed it is a known bug on MacOS.

Waiting for a fix, there are 2 workarounds:

  • Download the pack manually and install it using "From Local..." button from "Embedded Software Packages Manager" window. Or
  • If the project has been created through CubeMX standalone, you can install the pack from CubeMX.

Regards,

Florent

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
mattias norlander
ST Employee

In discussion with Florent, the ST internal ticket reference is: 119647.

Tried the 2 workarounds, ok for MacOS.

Thank you.