STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1549 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 588 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

(STM32F105C8, STM32CubeIDE 1.9.0, MacOS 11.6.5) Using STM32CubeIDE, how do I can't get TIM3 to tick/count when TIM2 overflows. (TIM2 does count up)

TIM2:Clock source: InternalMaster/Slave Mode: Disabled (Trigger input not delayed)Trigger Event Selection: Update EventTIM3:Slave Mode: Trigger ModeTrigger Source: ITR1TIM2 counts up like it should, but TIM3 doesn't count the over flow, but has incre...

FMoto.1 by Associate
  • 1695 Views
  • 2 replies
  • 1 kudos

Resolved! Failed to list external Loader

I try to add external loader to C:\ST\STM32CubeIDE_1.8.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.0.100.202110141430\tools\bin\ExternalLoaderIn debug configuration, check ExternalLodaer and than press Scan.Th...

ALomb.1 by Associate III
  • 8884 Views
  • 20 replies
  • 0 kudos
ltan.11 by Associate
  • 1780 Views
  • 1 replies
  • 0 kudos

Clicking on Search result opens the file in new Editor

Hi,This problem is observed in v1.9.0 as well as in earlier versions. If one clicks on any search result to open the respective line then the file is opened in a new Editor, despite the fact that the same file is already opened in another editor wind...

davhak by Associate II
  • 1497 Views
  • 4 replies
  • 0 kudos

Resolved! STM32Cube IDE app fails to run on latest macOS Monterey beta

I'm running the latest (less than one week old) macOS Monterey developer beta 12.4 (build 21F5063e) on a MacBook Pro 10,1 and downloaded the file en.st-stm32cubeide_1.9.0_12015_20220302_0855_x86_64.dmg_v1.9.0.zip, decompressed and installed the app. ...

0693W00000LzXVXQA3.png
mikew67 by Associate II
  • 2043 Views
  • 2 replies
  • 0 kudos

STM32CubeIDE 1.9.0 Question: User generated .c&.h files don't have the same functionality as the auto generated files like main.c.

I can add my own .ch files to a project and build and see the proper functionality on the MCU with no problems. However, the user generated src modules are not colorized, or system calls are not "Auto Complete" enabled like main.c module is. More imp...

FAssa.1 by Associate
  • 1144 Views
  • 3 replies
  • 0 kudos