STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1549 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 588 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Unable to communicate between stm32 and as7262 sensor

I'm using stm32 discovery board and connecting with as7262 sensor. The datasheet for as 7262 sensor is https://ams.com/en/as7262I am unable to retrieve the data using I2C communication. I have uploaded my code below.#define AS7262_ADD 0x93 #define ST...

RSath.1 by Associate II
  • 4915 Views
  • 6 replies
  • 0 kudos

I am using STM32F7 series. I created httpd server ethernet project. I have web code which html,css,js. But my microcontrollers memory not enough for these codes. I need to use SD Card.

I need to put it my web codes (html, css, js) to SD Card. Also These codes need to work on SD Card. Because my web codes memory size is around 300MB. Normally I worked my code (basic html files) without SD Card. It needs converting to fsdata.c files....

KAnahar by Associate III
  • 2733 Views
  • 5 replies
  • 0 kudos

Resolved! How do I get GDB debug output to a file?

I'm debugging a problem on the target. The data I want to examine is in an array and can be easily seen in the Debugger console using "print output_data". I'd like this in a file to facilitate further host processing. When using gdb standalone I c...

SMoor.6 by Associate
  • 4754 Views
  • 2 replies
  • 1 kudos

Resolved! How can I know where a function is being used in STM32CubeIDE?

When I analyze a code that another guy made, I want to track where a function is used.I can see the definition of a function using open declaration but I cannot see where the function is used.STM32 has so many files. So, I cannot search for each of t...

KKIM.6 by Senior II
  • 4936 Views
  • 3 replies
  • 0 kudos