STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1418 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 558 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

place flash-related functions in the ram in st,32f030k6t6

estoy utilizando flash para escribir y leer mientras tengo un bluetooth conectado por serial DMA, cuando intento escribir en flash en la consola de stm32cubeide aparece "Target is not responding, retrying..." mientras que mi serial de dma con el blue...

jdo by Associate II
  • 2859 Views
  • 6 replies
  • 0 kudos

How to STOP the TARGET when the CUBE is stopped?

When I am in the EDITION mode in the CUBE IDE, I perceived that the TARGET is running the last downloaded program. In my TARGET it jeopardize several parts like EEPROM model (which I just made). Therefore, I would like to ask if someone know how to S...

JSILV.2 by Senior
  • 743 Views
  • 0 replies
  • 0 kudos

Resolved! How to open an existing project

Hello, I would like to open an existing project : But when I select .'project' I have this picture and I can't see the code : Do you know how to do ? Thank you for your helps Regards

0693W00000NsEjyQAF.png 0693W00000NsEk3QAF.png
DYann.1 by Senior II
  • 18776 Views
  • 6 replies
  • 0 kudos

Resolved! Indexer problem in STM32CUDEIDE 1.8 and 1.9

Hello dear friends,I have installed STM32CUBEIDE v1.7, v1.8 and v1.9. Since V1.8 the indexer can't find variables and functions in cube-generated files and throw this type of message."Could not find symbol 'blah blah' in index".This issue is really a...

I am working with CubeIDE 1.7.0 . I was to move my project on latest 1.9.0 version, but this version of CubeIDE is give me 500 errors . Do you know where I can download CubeIDE 1.3.1 again ?

stm32 cubeide 1.9.0 version gcc 10 compiler give me error in structures files but in 1.7.0 version of software gcc 9 all ok with structure.maximum error cover with the help of extern before variables and function but only problem in structure defini...

SKapa.1 by Associate II
  • 2765 Views
  • 5 replies
  • 0 kudos