STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1554 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 588 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Unable to update STM32IDE

Hi, i cannot update the STM32IDE firmware. I only get this error after a long time of being stuck in the update process at 36%

0693W00000UoGUlQAN.png

Complementary PWM issue

Hi there,I am generating 250khz PWM signal using STM32f401ccu6 (Blackpill) to drive high side and low side mosfets. I am using Timer 1 channel 1 along with its complementary PWM feature to utilize dead time feature. Currently I have generated the PWM...

0693W00000UoJxHQAV.png 0693W00000UoJxMQAV.png 0693W00000UoJxRQAV.png 0693W00000UoJxWQAV.png
Hari123 by Associate
  • 5479 Views
  • 4 replies
  • 0 kudos

Developing in CubeIDE on network drive - corruption.

I was initially getting away with developing on a network drive.However it has all started to come apart.If I attempt to create a new project while the %HOME%\STM32Cube\Repository is on a network drive I get things like "Unable to unzip firmware..."W...

PCamp.2 by Associate III
  • 3149 Views
  • 5 replies
  • 0 kudos

STM32L011 consumption variation

I am starting with the STM32L011 MCU (NUCLEO-L011K4 kit) and I want to use it for a very low-power application.I need an operating frequency of 65536Hz to generate a pattern on a GPI/O continuously.So I configured the STM32 in LowPower Run mode with ...

How do I add checksum to hex image in CubeIDE?

I whish to make a main application for use with a custom bootloader.The main application should be compiled to a hex file with all empty space above the app, filled with 0xFF and with some of the last bytes containing a checksum of the app image.I fo...

0693W00000UnoIXQAZ.png
FwMaker by Associate II
  • 2644 Views
  • 1 replies
  • 0 kudos

How Correctly COPY a Project?

After Pasting one Project, and allowing Uptading Reference Button, I tried to open the *ioc file which issued "error". Then, I had to rename to the newest Project name, then I was abble to open the *.ioc file. So, I might ask: Is it the correct "proj...

JSILV.2 by Senior
  • 1895 Views
  • 4 replies
  • 0 kudos