STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1554 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 588 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! st link server is required to launch the debug session

Hello,using: STM32CubeIDE 1.10.1 on Windows 10I have not used the debugger for a week or so, I didn't do any updates (okay, Win 10 probably has, managed by company...), but all of a sudden when I want to start a debug session, this message pops up:st...

LCE by Principal II
  • 25922 Views
  • 2 replies
  • 0 kudos

Resolved! Variable of type float not showing negative float values

I am reading data from a magnetic field sensor and storing it in a variable of type float. But what concerns is that I can't see the negative measurements on the debug window. When I store it in a int16_t variable the negative measurements show up....

Kolab by Senior
  • 7621 Views
  • 11 replies
  • 0 kudos

Resolved! STM32CubeIDE crashes on MacOS Ventura 13.0.1

I just upgraded to MacOX Ventura 13.0.1 from MacOS 12 last night, and now STM32CubeIDE 1.10.1 crashes about 8 1/2 minutes from app startup, consistently. This is on a 2019 Intel 16" MacBook Pro. The crash happens even if the app is left idle.Has anyo...

Why does .elf load fails when using STM32CubeIDE ?

Hello, I have a problem with STM32CubeIDE which fails to load my .elf file into the STM32F030K6 I am trying to debug, in either debug or run modes. Everytime, an error window pops up with following message: "Error in final launch sequence:Failed to e...

RLEP.1 by Associate II
  • 8392 Views
  • 5 replies
  • 0 kudos

STM32F030K6T6 with Si4703 on STM32CubeIDE?

Hi everybody.I 'm trying to make an Si4703 radio module work with an STM32F030K6T6 on STM32CubeIDE.I have found an example which is made with Coocox, I think. At https://github.com/LonelyWolf/stm32/tree/master/Si4703 but does not it work with STM32Cu...

Resolved! Definition of a array of char[] fails, if its size is > 8

Hello community,I use CubeIde to program my STM32 L051R6T6.Language is C.I do the following definition in a .c file:enum internalFaults{ internalFaultsTransmitPrepare, internalFaultsTransmit, internalFaultsWatchdogAlarm, internalFaultsTelegramsRx...

TheaArt by Associate III
  • 5071 Views
  • 9 replies
  • 0 kudos

Resolved! Storing and retrieving an STM32CubeIDE project in GitHub

I have a project (https://github.com/carlk3/Digital-Automotive-Generator-Voltage-Regulator) that I've been developing in STM32CubeIDE on (Ubuntu) Linux. Now I want to move it to STM32CubeIDE on Windows. I'm using GitHub for source code management (SC...

CKugl.1 by Senior II
  • 3422 Views
  • 3 replies
  • 0 kudos