STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1450 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 568 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

CubeIDE 2.0.0 and LOAD segment with RWX permissions

Hello,I moved an existing project from 1.14 to 2.0.0. To be clear I created a new workspace, then a new project in 2.0.0 in order to prevent any non relevant bit taken from 1.14 (at the project level) and copied only the source files from 1.14 to 2.0...

Kraal by Lead
  • 1488 Views
  • 10 replies
  • 3 kudos

Resolved! autocomplete (ctrl+space) doesn't run

Hello,I downloaded stm32cubeIDE 2.0 + stm32cubeMX but I'm having problem in auto complete function in main.cI tried https://community.st.com/t5/stm32cubeide-mcus/stm32cubeide-auto-complete-ctrl-space-is-not-working/td-p/342759but Parsing-based Propos...

Kram28_0-1763914964473.png Kram28_1-1763915583037.png
Kram28 by Associate II
  • 704 Views
  • 4 replies
  • 0 kudos

Included path seems to not be included everywhere

Hi,I am working on a preexisting TouchGFX projects, and i am trying to make it multicore so i am trying to build with OpenAMP to test if i didn't tweak wrong settings in CubeMXI added the path in Project > Properties > C/C++ General > Preprocessor In...

Resolved! STM32CubeIDE / MX configuring octoSPI in multiplexed Mode

Hello,In my project, i am using 2 octoSPI devices connected to my STM32H735. (IDE is STM32CUbeIDE V1.19.0)After migrating the Project to STM32CubeMX 6.15.0 it is not possible to configure the octoSPI in Multiplexed Mode anymore. The existing config f...

AZorn.1 by Associate III
  • 1110 Views
  • 7 replies
  • 3 kudos