STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1451 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 568 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32CubeCLT 1.20.0 released

We are pleased to announce that STM32CubeCLT 1.20.0 release is available. What is new in 1.20.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.0.0Update of Clang toolchain version 19.1.6Update of GCC 13.3.rel1Update ...

Aimen1 by ST Employee
  • 1074 Views
  • 0 replies
  • 0 kudos

Unable to start CubeIDE v2.0.0 on Windows 7

I have installed the latest IDE in my windows 7 laptop. The installation was successful. When I open the application, I face the following error: An error has occurred. See the log file ....\configuration\.Log file:!SESSION 2025-11-22 14:02:55.630 --...

GongGing by Associate
  • 944 Views
  • 3 replies
  • 3 kudos

Resolved! Unable to start STM32CubeIDE_2.0.0

Hello,I can not start STM32CubeIDE_2.0.0.I have the following error:D:\ProgramFiles\STMicroelectronics\STM32CubeIDE_2.0.0\STM32CubeIDE;;.C:\Users\Mich\.swt\lib\win32\x86_64\swt-win32-4966r5.dll: La procedure specifiee est introuvableCan't load librar...

MLe M.1 by Associate III
  • 620 Views
  • 5 replies
  • 3 kudos

Resolved! STM32G0 hardfault and signal handler FFFFFFF1

I'm trying to find the cause of a hard fault in my code. The problem repeatedly appears after a few or more minutes after starting the  code, sometimes not at all, sometimes every time at close startup after enabling interrupts, and somethimes after ...

Xme_0-1716273865159.png Xme_2-1716274145362.png
Xme by Associate II
  • 7195 Views
  • 9 replies
  • 3 kudos

Resolved! Colors in CubeIDE on Linux

Hi! I have Linux Mint 22.2. How can I configure CubeIDE colors so that all windows have a white background? Various combinations of Windows->General->Appearance settings allow you to achieve a maximum white background for all windows except the one w...

ADrub.1 by Associate III
  • 1977 Views
  • 8 replies
  • 0 kudos

Resolved! No recent launches (?)

HiDeleted all my first attempts, wanted a new clean start.Then imported the "Templates" part of the ST provided "stm32cubec0-v1-4-0" examples.But it won't run nor build (greyed out).It says "The selection cannot be launched, and there are no recent l...

Baldrick by Associate II
  • 779 Views
  • 4 replies
  • 0 kudos

Fix app icon size in macOS dock

I know this sounds super nitpicky, but the app icon on macOS is not sized per Apple's human interface guidelines.Can you fix the app icon on macOS so it looks like all other macOS apps?Thanks! 

stm32cubeide_icon.png

Resolved! NUCLEO-U575ZI-Q - Can't run any program using OpenOCD

I've been beating my head for a while trying to use OpenOCD to download my program to the chip, and I'm getting error messages which cite a write algorithm error (errors attached below). I'm not really too sure what I'm doing wrong, and would greatly...

lindt_1-1762964740315.png lindt_2-1762964808489.png lindt_3-1762964893044.png lindt_4-1762964919298.png
lindt by Associate II
  • 1346 Views
  • 5 replies
  • 3 kudos