STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1531 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 584 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32CubeIDE Silent/Noninteractive Install

I'm attempting to set up a CI pipeline to build firmware built in STM32CubeIDE, but I've not been able to get STM32CubeIDE installed via Dockerfile without manual intervention. Is there a silent install or a way to pre-accept the license agreements s...

MBand.3 by Associate III
  • 2892 Views
  • 1 replies
  • 0 kudos

Resolved! STM32_I2C_BMP_280

Hello Everyone, I am trying to interface BMP280 sensor using I2C with STM32F401 Discovery Board. My code gets compiled without any error and i have declared two global variable, Temperature and Pressure . when i debug using ST Link GDB sever I cannot...

APand.7 by Associate II
  • 3088 Views
  • 3 replies
  • 0 kudos

STM32CubeIDE 1.12.0 released

STM32CubeIDE 1.12.0 was released today on st.com as well as an in-tool update patch.What is new in 1.12.0?* Microcontroller and board lists aligned with STM32CubeMX v6.8.0 – Added the support for the STM32H5 series microcontrollers – Added the suppor...

Is it possible to add Doxygen to stm32cubeIDE

Hello everyone,I am working on a project using the STM32F407 µC in the process of developing my code and documenting it I wanted to integrate Doxygen inside the IDE and I'm not sure if it's possible if yes I would appreciate it if anyone can show me ...

MBHIR.12 by Associate
  • 6039 Views
  • 3 replies
  • 0 kudos

Resolved! CubeIDE cannot find header files after import

This is an issue i currently have with two differents project. After importing an error free project, the IDE have issue linking included files.When building i have "fatal error: FLASH_G0.h: No such file or directory" on the #include "foo.h" line, a...

rcard by Associate II
  • 12749 Views
  • 8 replies
  • 2 kudos

HardFault_Handler"Debug in STM32CubeIDE

 I am currently working on a project using the STM32F407G-DISC1 development board and STM32CubeIDE. The goal is to analyze the data and print the respiratory rate after continuously collecting ADC data for 10 seconds. However, I encountered some prob...

_legacyfs_online_stmicro_images_0693W00000bidi8QAA.png _legacyfs_online_stmicro_images_0693W00000bidh1QAA.png _legacyfs_online_stmicro_images_0693W00000bidiDQAQ.png
名孫.1 by Associate
  • 1716 Views
  • 0 replies
  • 0 kudos

Nucleo-H723ZG LwIP HardFault_Handler problem

I am using a NUCLEO-H723ZG board. To enable lwip, I need to enable CPU DCache. With the default settings, and further compilation and launch in STMCubeIde (latest version 1.12), the program always crashes with the error HardFault_Handler. All the sam...

MGaif.1 by Associate II
  • 5328 Views
  • 8 replies
  • 0 kudos

How can I duplicate a project in STM32CubeIDE?

I have a project in a workspace in STM32CubeIDE, generated with STM32CubeMX. I would like to duplicate the entire project, including the .ioc information, to use as the starting point for a new project. How can I do this? I am amazed that this top...

msch by Associate III
  • 21690 Views
  • 25 replies
  • 13 kudos