cancel
Showing results for 
Search instead for 
Did you mean: 

MCU Finder still doesn't work, despite the release notes saying that it was fixed.

AWarr.1
Associate

The 1.8 release notes claim that the wayland support bug was fixed, yet the mcu finder still doesn't work. Please reopen bug 77518 or fix the issue.

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Aymen CHAKROUN
ST Employee

Hi @AWarr.1​ ,

Can you please open the CubeIDE installation folder and right click the file 'stm32cubeide_wayland' and select 'Run as a Program'.

Regards,

Aymen.

Semer CHERNI
ST Employee

Hello @AWarr.1​ 

Did the proposition of @Aymen CHAKROUN​  came to help?

Kind regards,

Semer.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

As far as I can tell, this executable is only delivered with the generic linux build. I am using the rpm installer.