STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1565 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 593 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Installing CUBE IDE on Ubuntu 23.04

New to STM - so far 2 major complaints...  CUBE products are basically unreadable to me...  Using a light grey on white background makes CUBE MX, at least, non-useable - can't see any themes options. I did see that CUBE IDE supports themes so I tried...

CanHobby by Associate
  • 4478 Views
  • 2 replies
  • 1 kudos

Resolved! STM32F412G-DISCO Blank Screen Problem

Hi, I have tried programming and resetting this discovery Board but all I now get is this fuzzy grey screen as shown in the image is there anyway to do a hardware reset or is it a programming error? I just either want to reset the board back to its d...

Linkpad by Associate III
  • 1832 Views
  • 1 replies
  • 1 kudos

How to debug Lorawan from AN5481

Hi all,I'm working with a board build with STM32CubeWl, in the pdf file here section 5.3.1 it's say for debug swith the source code use APP_LOG, it's right in my source code I have APP_LOG, but my question is where is the output ? UART ? Form StLink ...

SBaro.11 by Associate III
  • 1224 Views
  • 1 replies
  • 0 kudos

CubeIDE open declaration leads to file.h

Hi everybody.Im using cubeide for a dual core mcu and when it generate code F3 keyboard button that opens declaration for that function will lead to the .h file. I want it to lead to the .c file.Once i did some changes to project properties c/c++ sym...

problem while programming Option Bytes to configure brown out

Hi,after I try to program option byte to configure brown out I can't  anymore reach the micro.I'm working with a STM32G071KBU3.I also try to connect to the micro using CUBE programmer. I get the error "target not found". Below my code.The instruction...

DAUSILI by Associate III
  • 2228 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.