STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1226 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 509 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Linker script puts bss into flash - why?

When I'm done compiling, the memory details show"FLASH";"0x08000000";"";"64 KB" ".ITCMSection";"0x00000000";"0x080002a0";"1.36 KB" ".isr_vector";"0x08000000";"0x08000000";"672 B" ".text";"0x08000810";"0x08000810";"29.19 KB" ".rodata";"0x08007cd0";"0x...

Resolved! IDE Version 2.0.0 - why remove MX ?

Why, oh why have you separated IDE and MX such that .ioc files can no longer be opened in IDE?I cannot imagine any benefits and it makes the IDE significantly worse, such that I've felt compelled to revert to version 1.19.0 ( go to Help -> About STM3...

jcslb by Associate
  • 8431 Views
  • 49 replies
  • 57 kudos

Problem with main.c as a linked file

Hi, I changed the location of the main.c file in my disk then reimported it in the project explorer as a linked file under the same path (under core/src). When I modify the .ioc file, save it and regerated the code, the changes of the peripheral conf...

melek_g by Associate
  • 84 Views
  • 2 replies
  • 2 kudos

Excessive extra projects being imported with new Cube

A couple of weeks ago STM32Cube disappeared off my computer. I went a got the install file for the most recent version (2.1.1). Since I have installed this when I try to import an old project into the workspace or use MX to generate code when trying ...

GTann1_0-1777535558488.png GTann1_1-1777535598806.png
GTann.1 by Associate III
  • 109 Views
  • 3 replies
  • 2 kudos

Install CubeIDE on Raspberry Pi 5

Has anyone had success installing the Cube IDE on a Raspberry Pi 5?  I first got the error message "Installation dir cannot be temporary one: /home/my_name/Downloads/makeself_dir_o70WRx"I tried various workarounds suggested by Gemini, ultimately crea...