2026-04-29 6:34 AM
I have installed version 13.3.rel1, clean the files and re compile the code :
I have a linker error "undefined reference" to a function although the function referenced in the files and declared in the H file who was included.
"
C:/ST/STM32CubeIDE_2.0.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.100.202509120712/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/bin/ld.exe: ./Core/Src/stm32u0xx_hal_msp.o: in function `HAL_PCD_MspInit':
C:/Users/../Electronics/../Software/USB_CDC_U0/USB_CDC_U0/Debug/../Core/Src/stm32u0xx_hal_msp.c:102:(.text.HAL_PCD_MspInit+0x4c): undefined reference to `MX_USB_CDC_Init'
collect2.exe: error: ld returned 1 exit status
make: *** [makefile:65: USB_CDC_U0.elf] Error 1
"make -j12 all" terminated with exit code 2. Build might be incomplete.
15:33:51 Build Failed. 2 errors, 0 warnings. (took 13s.995ms)
I have tried the following:
1. I have tried changing the file order in "path and symbols" clean and recompile - no success
2. I have tried changing the function name - - no success
3. I have deleted the object files in the debug section clean the code and re-compile - no success.
currently I am using version 13.3.rel1 of STM32 GNU and CubeIDE 2.1.1 tools downgraded from version 14.3.rel1 due to other errors encountered while compiling the code - see the link below:
I have attached the code
Please help
UVC100
Solved! Go to Solution.
2026-05-03 11:48 PM
Hi Andrew ,
Thank you for light me the way ,
The code in the USB directory was not compiled, although it was part of the software ,
All the code must be placed under the core directory , otherwise it will not be recognized, compiled or linked
thank you
UVC100
2026-04-29 6:49 AM
Are you sure that the source file containing the definition (not just the prototype) of MX_USB_CDC_Init is actually included in the build?
Does the CubeIDE 'Go To Definition' find it?
2026-04-29 11:58 PM
Hi Andrew,
In the last test I done , I change the name of function, thought the name is to long , it has no effect the on the result - same linker error.
Please see below the text from the updated function name :
"C:/ST/STM32CubeIDE_2.0.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.100.202509120712/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/bin/ld.exe: ./Core/Src/stm32u0xx_hal_msp.o: in function `HAL_PCD_MspInit':
C:/Users/../Hardware - General/../../Software/USB_CDC_U0/USB_CDC_U0/4c): undefiDebug/../Core/Src/stm32u0xx_hal_msp.c:102:(.text.HAL_PCD_MspInit+0xned reference to `MX_USB_INIT'
collect2.exe: error: ld returned 1 exit status
make: *** [makefile:65: USB_CDC_U0.elf] Error 1
"make -j12 all" terminated with exit code 2. Build might be incomplete."
The function current name is :MX_USB_INIT()
the function located in the USB_CDC_IF.c file (see attached code)
the function Exported in the in the USB_CDC_IF.h
call to the function done in the STM32U0xx_hal_msp.c within the function HAL_PCD_MspInit()
USB_CDC_IF.h was included in the STM32U0xx_hal_msp.c file
Thank you
2026-04-30 2:26 AM
@UVC100 wrote:the function located in the USB_CDC_IF.c file (see attached code)
And are you sure that file is actually being built ?
2026-05-03 11:48 PM
Hi Andrew ,
Thank you for light me the way ,
The code in the USB directory was not compiled, although it was part of the software ,
All the code must be placed under the core directory , otherwise it will not be recognized, compiled or linked
thank you
UVC100
2026-05-05 3:03 AM
Glad to hear it's now fixed!
But note that this is not true:
@UVC100 wrote:All the code must be placed under the core directory , otherwise it will not be recognized, compiled or linked
It certainly is possible to have code outside the 'Core' folder which does get included in the build.